Handeling event that triggers when Solid Edge is minimazed

Valued Contributor
Valued Contributor

Does any one knows any handeling event that triggers when Solid Edge is minimazed?

 

Thanks

Sergio

 

 

Posted by: Sergio Vallejo
Post date: 9/1/2011 4:59:16 AM

2 REPLIES

RE: Handeling event that triggers when Solid Edge is minimazed

Valued Contributor
Valued Contributor

Hi Sergio,

 

this should be possible by consuming the ApplicationWindowEvents.WindowProc event and providing an event handler for it. But i did not success to use this event, since it seems that offering an event handler for the event WindowProc keeps the Window Messages from being passed through Solid Edge any more. I don't see any documented procedure or example how to pass through the Window Messages to Solid Edge to get them processed by Solid Edge as usual.

 

Posted by: Wolfgang Kunert
Post date: 9/4/2011 9:45:40 PM

RE: Handeling event that triggers when Solid Edge is minimazed

Valued Contributor
Valued Contributor

I could be wrong but I believe you must return E_NOTIMPL if you don't handle the event. In .NET terminology, that means throwing a new System.NotImplementedException.

 

Posted by: Jason Newell
Post date: 9/4/2011 10:16:16 PM