Cancel
Showing results for 
Search instead for 
Did you mean: 

HoleData of an AssemblyFeaturesHole object

Pioneer
Pioneer

Hi all,

 

I am having problems to change the HoleData in an assembly like in the part environment. To get to the hole I go through the AssemblyFeaturesHoles collection in the AssemblyFeatures. The name of the hole object matches the object in the pathfinder.

 

However unlike in the part environment the hole does not have a HoleData property but a method. Unfortunately I only get an exception but not the HoleData object.

 

Even in the HoleDataCollection there is no HoleData object. I am stuck at this point. Any ideas?

 

Robin

 

 

3 REPLIES

Re: HoleData of an AssemblyFeaturesHole object

Pioneer
Pioneer

Anyone?

Re: HoleData of an AssemblyFeaturesHole object

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

This is on one hand missing API support and on the other hand not exposed information of "manually" created feature info to the API.

If you really need this functionality, request it through an Incident Report.

Re: HoleData of an AssemblyFeaturesHole object

Pioneer
Pioneer

I feared that you might write that (but hoped that I made a mistake and it is already possible). Thanks for the clarification though.