Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I extract these dimension entries from the variable table

Experimenter
Experimenter

Hello,

 

I have an assembly in which 2 parts are included. I aligned the 2 parts in parallel. This insert dimension entries in the variable table.

How can I extract these dimension entries from the variable table by program.

 

Thank you for any help you can give

Pepper

2 REPLIES 2
Highlighted

Re: How can I extract these dimension entries from the variable table

Gears Phenom Gears Phenom
Gears Phenom

@Pepper 

 

Please be sure to see  the pinned post "Useful Solid Edge Developer Community Links"

 

Therein you will find the GitHub link to "Solid Edge Samples

 

Within the "Solid Edge Samples" is an example of "GetVariables"

 

HTH

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: How can I extract these dimension entries from the variable table

Experimenter
Experimenter

Matt,

Thank you for the fast answer. "GetVariables" helped me a lot. I would never have come up with the Query method.

Best regards
Pepper