Cancel
Showing results for 
Search instead for 
Did you mean: 

How do i use the command "SaveAsToTeamCenter"?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello, i've tried to use this command to copy a item from teamcenter to another "Item ID", but nothing happens, i also tried to give a "Save As" direct to the SEEC Cache, the item is created in teamcenter, but the dataset names are with the wrong revision.

 

I'm using Solid Edge ST7 MP8.

 

Code:

 

Dim objListFileNames As Object = Nothing

Set objSolidEdgeTCE = objApplication.SolidEdgeTCE

Call objSolidEdgeTCE.SaveAsToTeamCenter("9999", "A", "9999/A", "Latest Working", "PEC", objListFileNames)

 

1 REPLY

Re: How do i use the command "SaveAsToTeamCenter"?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I recommend that you submit an IR with GTAC. If you get an answer, please reply back to this thread and give us an update.

Jason Newell
Applications Architect
www.jasonnewell.net