Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to check settings in the Solid Edge Options C#

Valued Contributor
Valued Contributor

Hello together,

 

it's my first post here an i am starting with an question.

 

I want to write a little program in C# and do it step by step...it's my way to learn about programming Solid Edge.

 

So the question is how can i check in the Assembly-Environment which options are set for the Itemnumber in the active assembly.

 

I work with Solid Edge ST4.

 

Maybe someone kann give me a Codesnippet!??

 

Greets Markus

 

Posted by: Markus Schwaning
Post date: 5/15/2012 6:03:23 AM

1 REPLY 1

Re: How to check settings in the Solid Edge Options C#

Valued Contributor
Valued Contributor

Hi,

 

unfortunately options aren't accessible via a centralized method and reading them requires (if they are exposed via the API at all) searching them in the properties of objects spread all over the Solid Edge API.

I also was unable to locate the setting you search for :-(

 

Posted by: Wolfgang Kunert
Post date: 5/23/2012 4:25:15 AM