Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create Assembly Patterns?

Valued Contributor
Valued Contributor

 

From the API reference it is not clear how to use function AssemblyPatterns.Create( PatternName, MasterOccurrences, FeaturePattern, ReferenceFeature) and what arguments to pass.

I used the following sample in VB to create a new AssemblyPattern but it always failed.

Dim objOccArray(1 To 1) As Object

Set objOccArray(1) = objAssmDoc.Occurrences(2)

Dim Occ As SolidEdgeAssembly.Occurrence

Occ = objAssmDoc.Occurrences(1)

Dim objPart As SolidEdgePart.PartDocument

objPart = Occ.OccurrenceDocument       

objPattern = objPart.Models(1).Patterns.Item(1)

HoleObj = objPart.Models(1).Holes(1)

objAsmPattern = objAssmDoc.AssemblyPatterns.Create("MyPattern", objOccArray, objPattern, HoleObj) 

I also tried to get parameters from already existing AssemblyPattern and used them to create another AssemblyPattern. To get parameters I used function AssemblyPatterns.GetInputs( ... ). Then I deleted the old AssemblyPattern and tried to create a new one using the retrieved parameters. But AssemblyPatterns.Create(...)  failed again.

Thanks

 

Posted by: Sergey Sergeenko
Post date: 1/12/2010 10:57:50 PM

8 REPLIES

RE: How to create Assembly Patterns?

Valued Contributor
Valued Contributor

 

Hi Sergey,

 

your way is good, but your objects are from Part and not from Assembly. You must create references extra for the Assembly:

 

Dim objRefPattern as Object

objRefPattern = objAssmDoc.CreateReference(Occ, objPattern)

Dim objRefHole as Object

objRefHole = objAssmDoc.CreateReference(Occ, HoleObj)

'and

objAsmPattern = objAssmDoc.AssemblyPatterns.Create("MyPattern", objOccArray, objRefPattern, objRefHole)

 

Regards

JR

 

Posted by: JR
Post date: 1/17/2010 11:47:42 PM

RE: How to create Assembly Patterns?

Valued Contributor
Valued Contributor

You are absolutely right!

It's supposed from the definition of the method that the arguments must be reference-objects

The only problem that creating reference of feature has always failed (At least I couldn't do that)

 

Thanks

 

Posted by: Sergey Sergeenko
Post date: 1/19/2010 1:29:26 AM

RE: How to create Assembly Patterns?

Valued Contributor
Valued Contributor

By me is all OK. Can you copy the coding hier?

 

Posted by: JR
Post date: 1/19/2010 6:16:32 PM

RE: How to create Assembly Patterns?

Valued Contributor
Valued Contributor

Here is my test code

 

Dim Occ1 As SolidEdgeAssembly.Occurrence

Occ1 = objAsmDoc.Occurrences.Item(1)

 

Dim PartDoc As SolidEdgePart.PartDocument

PartDoc = Occ1.OccurrenceDocument

 

Dim Hole As SolidEdgePart.Hole

Hole = PartDoc.Models.Item(1).Holes.Item(1)

Dim AsmHole As Object

AsmHole = objAsmDoc.CreateReference(Occ1, Hole) 'exception E_FAIL

 

Dim Pattern As SolidEdgePart.Pattern

Pattern = PartDoc.Models.Item(1).Patterns.Item(1)

Dim AsmPattern As Object

AsmPattern = objAsmDoc.CreateReference(Occ1, Pattern) 'exception E_FAIL

 

 

 

 

Posted by: Sergey Sergeenko
Post date: 1/19/2010 9:57:33 PM

RE: How to create Assembly Patterns?

Valued Contributor
Valued Contributor

I don't have any problems with your code!

 

Posted by: JR
Post date: 1/20/2010 12:38:26 AM

RE: How to create Assembly Patterns?

Valued Contributor
Valued Contributor

It's really strange...

Probably it depends on the version of Solid Edge( My version is 20.00.00.96 )

 

 

 

 

 

Posted by: Sergey Sergeenko
Post date: 1/20/2010 2:19:21 AM

RE: How to create Assembly Patterns?

Valued Contributor
Valued Contributor

 

My version is 20.00.15.05. Try again after instalation of Service Pack 15.

 

Posted by: JR
Post date: 1/20/2010 6:09:57 PM

RE: How to create Assembly Patterns?

Valued Contributor
Valued Contributor

 

After installing SP15 Solid Edge all the time throws exception when I call the method

 

Dim Occs As SolidEdgeAssembly.Occurrences

Occs = objAsmDoc.Occurrences

 

I even don't know what to do... probably somehow initialize assembly or something else

 

Posted by: Sergey Sergeenko
Post date: 1/22/2010 10:02:14 PM