Cancel
Showing results for 
Search instead for 
Did you mean: 

How to get the Assembly level features in c++

Valued Contributor
Valued Contributor

 

When we are trying to get the Assembly feature count and traversing for each feature details... the program is getting crashed... please let me know the proceeding

 

Posted by: Triad User
Post date: 4/27/2009 1:52:01 AM

4 REPLIES 4

RE: How to get the Assembly level features in c++

Valued Contributor
Valued Contributor

I'd be glad to help you but I need to see your code first. At least give me a demo snippet of the crash.

 

Posted by: Jason Newell
Post date: 4/27/2009 7:30:27 AM

RE: How to get the Assembly level features in c++

Valued Contributor
Valued Contributor

 

 Hi Jason,

  Thank you very much for the quick responce... i  hope the problem will be solved  soon.

 Note : I am using Solid Edge V 18.0

//*** I have attached the code... and i am uploading the test file also... please check with this... i have written the comments also ...where it is crashing

int _tmain(int argc, TCHAR* argv[], TCHAR* envp[])

{

 

 HRESULT hres=S_OK;

 

 ApplicationPtr pSEApp = NULL;

 

 hres = CoInitialize(NULL);

 

 if (FAILED(pSEApp.GetActiveObject("SolidEdge.Application")))

 {

  // Dont have Solid Edge running. Create a new instance.

  HRESULT hr = pSEApp.CreateInstance("SolidEdge.Application");

  if(FAILED(hr))

  {

   ::MessageBox(0,"Failed to create an instance of Solid Edge",0,0);

   return -1;

  }

 

  pSEApp->PutVisible(VARIANT_TRUE);

 

 }

 if(pSEApp == NULL)

  return -1;

 

 DocumentTypeConstants nDoctype = pSEApp->GetActiveDocumentType();

 if(nDoctype == igAssemblyDocument)

 {

  IDispatchPtr pDisp = pSEApp->GetActiveDocument();

  //Process for the Assembly feature traversing

  AssemblyDocumentPtr pAsmDoc=(AssemblyDocumentPtr)pDisp;

 

  AssemblyFeaturesPtr pAsmFeat=pAsmDoc->GetAssemblyFeatures();

 

  //AssemblyFeaturesExtrudedCutouts information

  AssemblyFeaturesExtrudedCutoutsPtr pAsmFeatExtCuts = pAsmFeat->GetAssemblyFeaturesExtrudedCutouts();

  if(pAsmFeatExtCuts)

  {

   long nAsmFeatCnt = pAsmFeatExtCuts->GetCount();

   for(long l=1;l

   {

    //Application is getting crashed while getting 'AssemblyFeaturesExtrudedCutout"

    AssemblyFeaturesExtrudedCutoutPtr pAsmFeatExtCut= pAsmFeatExtCuts->Item(l);

   }

  }

 }

 

 return 0;

}

 

 

Posted by: Triad User
Post date: 4/27/2009 6:29:30 PM

RE: How to get the Assembly level features in c++

Valued Contributor
Valued Contributor

 

Not sure why yours is failing.  I pasted my code below and I also attached the solution.  I ran my example in Solid Edge ST.// AssemblyFeaturesExtrudedCutouts.cpp : Defines the entry point for the console application.//#include "stdafx.h"int _tmain(int argc, _TCHAR* argv[]){ HRESULT hr = S_OK; SolidEdgeFramework::ApplicationPtr pApplication = NULL; SolidEdgeFramework:Smiley FrustratedolidEdgeDocumentPtr pDocument = NULL; SolidEdgeAssembly::AssemblyDocumentPtr pAssembly = NULL; SolidEdgeAssembly::AssemblyFeaturesPtr pAssemblyFeatures = NULL; SolidEdgeAssembly::AssemblyFeaturesExtrudedCutoutsPtr pAssemblyFeaturesExtrudedCutouts = NULL; SolidEdgeAssembly::AssemblyFeaturesExtrudedCutoutPtr pAssemblyFeaturesExtrudedCutout = NULL; IfFailGo(CoInitialize(NULL)); IfFailGo(pApplication.GetActiveObject(_T("SolidEdge.Application"))); pDocument = pApplication->ActiveDocument; IfNullGo(pDocument); if (pDocument->Type == SolidEdgeFramework::igAssemblyDocument) { pAssembly = pDocument; pAssemblyFeatures = pAssembly->GetAssemblyFeatures(); pAssemblyFeatures->GetAssemblyFeaturesExtrudedCutouts(); pAssemblyFeaturesExtrudedCutouts = pAssemblyFeatures->GetAssemblyFeaturesExtrudedCutouts(); for (LONG i = 1; i Count; i++) { pAssemblyFeaturesExtrudedCutout = pAssemblyFeaturesExtrudedCutouts->Item(i); _bstr_t bstrName(pAssemblyFeaturesExtrudedCutout->Name); _tprintf(_T("%s\r\n"), bstrName.GetBSTR()); } }Error: pAssemblyFeaturesExtrudedCutout = NULL; pAssemblyFeaturesExtrudedCutouts = NULL; pAssemblyFeatures = NULL; pAssembly = NULL; pDocument = NULL; pApplication = NULL; CoUninitialize(); return 0;}

 

Posted by: Jason Newell
Post date: 4/29/2009 12:14:35 PM

RE: How to get the Assembly level features in c++

Valued Contributor
Valued Contributor

 

Hi Jason,

  Thank you very much for the reply, i checked your code also in Solid Edge V 18.0, it is failing...  So i want to check it in Solid Edge ST. I will back to you soon.

 

Posted by: Triad User
Post date: 4/29/2009 6:48:32 PM