Cancel
Showing results for 
Search instead for 
Did you mean: 

How to get the parent edge of the DVLine in DrawingView

Valued Contributor
Valued Contributor

 

HI,

    How can I find the parent edge of an dvline in drawingview.

bye.

 

Posted by: Pritam Dulam
Post date: 11/16/2009 8:29:58 PM

1 REPLY

RE: How to get the parent edge of the DVLine in DrawingView

Valued Contributor
Valued Contributor

It is not possible, as far as i know. I think that there is not a relation exposed because a DVLine can come from an edge or not.

For example, a front view from a cylinder is a rectangle, the vertical lines does not exist in the model, they are the silouette representation of the cylinder body.

In the past someone else asked something similar. He wanted to retrieve the Feature in the 3D body, and i guess the answer is the same:

A DVLine can come from an edge belonging to a feature or can be a consecuence of an intersection between features, for instance.

So i guess (personally, not documented) that they didn't expose any method to retrieve relations between DVlines and 3D because of the "internal complexity" that could be on this.

Sorry, bad news

Julian

 

Posted by: Julian Guillo
Post date: 11/23/2009 9:08:20 PM