Cancel
Showing results for 
Search instead for 
Did you mean: 

INSIGHT - Need Excel VB Macro to export Insight Data

Valued Contributor
Valued Contributor

 

HI!

does someone have code to export data from insight.

Tried something like this in excel, but does not work!

Dim objApplication As RevisionManager.Application

Dim objInsight As RevisionManager.Insight

Sub Main()

 

    Dim aListOfDocumentsToExport() As Object

    Dim ExportToLocation As String

    Dim SetDocToReadOnly As Boolean

    Dim OverWriteOption As Boolean

 

    Dim c As Collection

    Dim sr As Integer

 

    sr = FreeFile

'Filelist is tezt file, with a list of documents to export, like http://server/site/par1.par etc.

    FileList  = Sheets("Sheet1").Range("FileList").Value

    Destination = Sheets("Sheet1").Range("Destination").Value

 

    Open FileLIst For Input As #sr

    Dim l As String

    Dim Step As Integer

    Step = 100

    While Not EOF(sr)

 

        Call ConnectRevisionManager

 

        Set c = New Collection

        'Get list of items to export

        For i = 1 To Step

            If Not EOF(sr) Then

                Line Input #sr, l

                c.Add (l)

            End If

        Next

        ReDim aListOfDocumentsToExport(c.Count)

 

        ExportToLocation = Destination

        SetDocToReadOnly = False

        OverWriteOption = RevisionManager.OverWriteFilesOption.YesToAll

 

        Call objInsight.ExportDocumentsFromServer(c.Count, c, ExportToLocation, SetDocToReadOnly, OverWriteOption)

 

        Call DisconnectRevMgr

 

        c = Nothing

 

    Wend

 

    Close (sr)

 

    End Sub

Sub ConnectRevisionManager()

 

    On Error Resume Next

 

    Set objApplication = GetObject(, "RevisionManager.Application")

 

    If Err Then

        ' Solid Edge is not running.  Clear the previous error.

        Err.Clear

        ' Start Solid Edge RevMgr.

        Set objApplication = CreateObject("RevisionManager.Application")

 

        ' Cannot start Solid Edge, so exit the program.

        If Err Then

            MsgBox "Cannot start Solid Edge.", vbCritical + vbOKOnly, "Open & Save"

            End

        End If

 

    End If

    On Error GoTo 0

 

    ' Get reference to Insight object.

    Set objInsight = objApplication.Insight

End Sub

Sub DisconnectRevMgr()

    ' Release COM Objects.

    If Not (objInsight Is Nothing) Then

        objInsight = Nothing

    End If

    If Not (objApplication Is Nothing) Then

        objApplication = Nothing

    End If

End Sub

 

I need to use VB in excel since have no way to install Visual Studio Express or similar.

Thanks in advance for any info.

Best Regards

Massimo

 

Posted by: Massimo Magris
Post date: 5/13/2010 8:41:32 PM

1 REPLY

RE: INSIGHT - Need Excel VB Macro to export Insight Data

Valued Contributor
Valued Contributor

 

Massimo,

Can you be little more specific about what exactly you are trying to achieve, what problem you are facing with the current code and where (the specific line in the code if possible)?

 

 

Posted by: Sanjay Kulkarni
Post date: 5/19/2010 12:21:20 AM