Cancel
Showing results for 
Search instead for 
Did you mean: 

Is possible to add a scripting engine to SolidEdge?

Valued Contributor
Valued Contributor

 

HI,

since SolidEdge does not have VBA, it's possible to create an addin to run scripts or macro from SolidEdge?

Example VB net or C# script?

There is something like that already done?

This should be a standard feature for a CAD, since all the major competitors have it.

Thanks for any info.

Best Regards

Massimo

 

 

 

Posted by: Massimo Magris
Post date: 3/4/2009 12:02:24 PM

1 REPLY

RE: Is possible to add a scripting engine to SolidEdge?

Valued Contributor
Valued Contributor

I had prototyped one out for PowerToys for Solid Edge but never finished it. I would love to get back to it some day. I would say that it is certainly possible and I see it as something that I would like to add to my free product line.

 

Posted by: Jason Newell
Post date: 3/4/2009 3:57:00 PM