Cancel
Showing results for 
Search instead for 
Did you mean: 

It-s possible to create a "custom/user defined" SolidEdge Command

Valued Contributor
Valued Contributor

 

HI,

It's possible to define a "custom/user defines" command, that can be called by

void StartCommand(

    SolidEdgeCommandConstants CommandID

)

Thanks in advance, best regards

Massimo

 

Posted by: Massimo Magris
Post date: 2/19/2009 2:14:59 AM

1 REPLY 1

RE: It-s possible to create a "custom/user defined" SolidEdge Command

Valued Contributor
Valued Contributor

Massimo,

 

When you call SetAddInInfo(), the last parameter is an array of command id's that Solid Edge assigns to your addin for the specific environment. Problem is, these id's are dynamically created and are not static like the standard commands.

 

So, technically speaking, you can call StartCommand() on any of your assigned id's.

 

Posted by: Jason Newell
Post date: 2/22/2009 7:29:48 PM