Cancel
Showing results for 
Search instead for 
Did you mean: 

Iterating through Synchronous features

Valued Contributor
Valued Contributor

Hi,

 

I am trying to fetch all the features present in part. Part may be synchronous or ordered.

 

I am trying below C# code.

 

SolidEdgePart.Features PartFeatures = ModelObj.Features;

int FeatureCount = PartFeatures.Count;

 

if (FeatureCount > 0)

{

for (int i = 1; i <= FeatureCount; i++)

{

object FeatureObj = PartFeatures.Item(i);

 

System.Type AType = FeatureObj.GetType();

 

string SEName = AType.InvokeMember("Name", System.Reflection.BindingFlags.GetProperty, null, FeatureObj, null) as string;

}

}

 

Above code gives me the name of features if the part has ordered features but in case of synchronous it just gives me faceSet_1 etc.

 

How should I get the name of the features in synchronous mode?

 

Posted by: sandeep
Post date: 8/14/2012 3:49:09 AM

1 REPLY

Re: Iterating through Synchronous features

Valued Contributor
Valued Contributor

Hi sandeep

 

i'm no expert in C# but i don't think that there is a problem here.

as i understand it, in sync par the feature is created as face_set.

therefore .name and .displayname and .systemname are "face set..." while their .edgebarname is protrusion1 etc.

does it help in any way??

 

Alon B)

 

Posted by: alon raviv
Post date: 8/18/2012 7:39:11 AM