Cancel
Showing results for 
Search instead for 
Did you mean: 

Link behaviour change in ST9 with LinkMgmt.txt and document freezing

Builder
Builder

Hi there!

 

Since our update to ST9, we have been experiencing some changes in the link management of the files and their drafts, or at least in its behaviour.

 

In our workflow, all drafts are always stored in a 'DRAFTS' subfolder placed where the parts of the machine are. So for example, the placement of a component along its draft is as follows:

 

//arbitrary_path/machine_folder/component1.par
//arbitrary_path/machine_folder/DRAFTS/component1.dft

 

As we move projects from disc to network and so on, 'arbitrary_path' can change, but the relative link between a component and its draft is not changed, at least as far as we don't change 'DRAFTS' name.

 

We use the default LinkMgmt.txt configuration, so no break link should occur if we just change 'arbitrary_path', since the RELATIVE approach should work fine. In fact, in previous versions of SE, even changing DRAFTS with another name was fine. SE seemed smart enough to find for a link inside a draft in the upwards folder before trying to get the absolute path.

 

From our experience, SE has lost that 'look upwards' behaviour and, even more, when the RELATIVE paths have not changed, sometimes (not always, weird!) the links are broken and we must make a full re-link.

We have tried a dirty trick in order to get back the 'look upwards' of the past, editing LinkMgmt.txt this way:

 

 

CONTAINER
RELATIVE
ABSOLUTE
BEGIN SEARCH PATH
..
..\..
END SEARCH PATH

 

As you can see, we have added instructions to look in the up folder until two depth levels (sometimes we make subfolders for diferent drafts, so a second level in the tree is useful). To our surprise this works :-D, althought, as I said, nothing of this was ever needed in previous versions. SE managed to reach links placed in upper levels naturally.

 

Now comes the amazing part of the story: with the LinkMgmt.txt as shown, whenever we try to launch SE and open documents through the API, the whole app gets freezed. No errors, no exception, no messages. SE gets freezed and the document never opens. If we have manually launched SE before, so it's not opened from the API, we can skip the freeze most of the time, but not always.

 

If we restore LinkMgmt.txt to its default, all works fine.

 

Conclusion: launching SE and opening documents from the API does not like our 'seek upwards' tricky directives, which in fact work superb when working manually, althought were not never needed in older versions of the software.

 

The opening and loading of documents it's done by means of the typical API methods:

 

Activator.CreateInstance(Type.GetTypeFromProgID("Solidedge.Application")
Application.Documents.Open("full_path_of_my_draft")

 

If it's difficult to understand all this, try to guess how tricky it as until we could define this odd behaviour. Can anyone throw some light over this?

 

Thanks for your time and patience if you were ever able to get here. Hope this can be useful for someone.