Make base feature from construction body

Valued Contributor
Valued Contributor

 

Hi, when I import certain SAT files into solid edge, it imports into the part file as a series of part copy construction bodies. I then have to manually go into the file and make the base feature. I want  to write a program (c#) that can do this automatically.

Can anyone suggest an interface or method that will take a construction body and convert it to a body feature. The same way make base feature does in one command.

Thanks

Jasno

 

Posted by: jason valverde
Post date: 1/28/2009 12:53:40 PM