Material list

Valued Contributor
Valued Contributor

Hi all,

 

I need to read the density of a material in SE V17, but I can't!

 

Who can help me?

 

My code is:

 

Option Explicit

 

Private Sub Form_Load()

Dim objApp As SolidEdgeFramework.Application

Dim objMaterialTable As SolidEdgeFramework.MatTable

 

Dim NumMat As Long

Dim listOfMat As Variant

Dim PROP As String

Dim J As Integer

 

On Error GoTo Errore

Set objApp = GetObject(, "solidedge.application")

objApp.Visible = True

Set objMaterialTable = objApp.GetMaterialTable

 

Call objMaterialTable.GetMaterialList(NumMat, listOfMat)

 

For J = 0 To NumMat - 1

Debug.Print J & " " & listOfMat(J)

Next J

 

Call objMaterialTable.GetMatPropValue(listOfMat(48), seModulusElasticity, PROP)

Debug.Print PROP

 

 

Set objMaterialTable = Nothing

Set objApp = Nothing

 

Exit Sub

Errore:

Call MsgBox(Err.Description, vbOKOnly + vbInformation, "ERRORE")

End

 

End Sub

 

Posted by: Delki Trolese
Post date: 11/13/2005 10:08:43 PM

3 REPLIES

RE: Material list

Valued Contributor
Valued Contributor

Hi Delki,

 

The density is a variable on SE part/sheetmetal

 

"PhysicalProperties_Density"

 

I think you could read the density of each part on the asm

 

borja

 

 

Posted by: pepe perez
Post date: 11/13/2005 10:36:44 PM

RE: Material list

Valued Contributor
Valued Contributor

Hi Borja

 

I can read the density in phisical property AFTER I put in the material.

 

I'writing a macro to process a lot of files to put in them the material and the density, and update the mass of any files PAR/PSM and ASM.

 

So I need to read the density from the materila.mtl

 

Best regards

Delki Trolese

Italy

 

Posted by: Delki Trolese
Post date: 11/13/2005 11:36:59 PM

RE: Material list

Valued Contributor
Valued Contributor

I haven't worked with the material table, but I do have a program that reads the density and updates the physical properties. Here is a snippet of reading the density:

 

objPartDoc = theEdge.ActiveDocument

objModels = objPartDoc.Models

If objModels.Count >= 1 Then

objModel = objModels.Item(1)

objPartDoc.GetGlobalParameter(SolidEdgePart.PartGlobalConstants.sePartGlobalDensity, dblDensity)

If dblDensity = 0.0# Then

MsgBox("The density is currently set to 0. Please verify the material and density.", MsgBoxStyle.OKOnly)

If Not (objModel Is Nothing) Then

Marshal.ReleaseComObject(objModel)

End If

End If

End If

 

Here is updating physical properties for a part file:

 

objModel.ComputePhysicalProperties(dblDensity, 0.999, oVolume, oArea, oMass, oCenterOfGravity, oCenterOfVolume, oGlobalMoments, oPrincipalMoments, oPrincipalAxis1, oRadiiOfGyration, 0.001, oUpdateStatus)

 

I'll attach a subroutine I wrote in an addin.

 

Good luck,

Mike

 

 

Here is updating physical properties for an assembly file:

objAssemblyDoc.PhysicalProperties.Update()

 

 

Posted by: Michael Frayser
Post date: 11/14/2005 8:02:48 AM