Cancel
Showing results for 
Search instead for 
Did you mean: 

Matrix methods

Valued Contributor
Valued Contributor

The occurrence class has a method GetMatrix() which gives a matrix for converting from part coordinates to assembly coordinates and back.  But this yields a 16 array, and I see no methods for using this matrix.  Given there are different ways it could be encoded, I hope somewhere there are methods for multiplying these matrices together, and transforming points.  Anyone?

------------------
Alan Baljeu
Owner, Cornerstone Intelligent Software
Developer of custom CAD software
6 REPLIES 6

Re: Matrix methods

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Alan,

 

I am by no means a matrix expert but I do know there are plenty of 3rd party libraries for handling matrices. Solid Edge leaves it up to you to choose the library of your choice or roll your own. I've worked with math gurus in the past who totally got Solid Edge matrices and had no issue working with them. They knew what they were doing though and I don't...

 

I threw together a small demo of 2 free libraries that I'm familar with. OpenTK & SharpGL. Again, I don't for a second pretend that I know how to use them. Just sharing what I do know.

 

using SolidEdgeCommunity;
using SolidEdgeCommunity.Extensions;
using System;
using System.Collections.Generic;
using System.Linq;
using System.Text;

namespace MatrixDemo
{
    class Program
    {
        [STAThread]
        static void Main(string[] args)
        {
            OleMessageFilter.Register();

            var application = SolidEdgeUtils.Connect();
            var assembly = application.GetActiveDocument<SolidEdgeAssembly.AssemblyDocument>();
            var occurrences = assembly.Occurrences;

            foreach (var occurrence in occurrences.OfType<SolidEdgeAssembly.Occurrence>())
            {
                // Allocate array.
                Array matrix = Array.CreateInstance(typeof(double), 16);

                // Get the occurrence matrix.
                occurrence.GetMatrix(ref matrix);

                // Convert Array to double[] for ease of use.
                double[] m = matrix.OfType<double>().ToArray();

                // NuGet package id: OpenTK
                DemoOpenTK(m);

                // NuGet package id: SharpGLCore
                DemoSharpGL(m);
                
            }

            OleMessageFilter.Unregister();
        }

        static void DemoOpenTK(double[] m)
        {
            
            var matrix4d = new OpenTK.Matrix4d(
                m[0],
                m[1],
                m[2],
                m[3],
                m[4],
                m[5],
                m[6],
                m[7],
                m[8],
                m[9],
                m[10],
                m[11],
                m[12],
                m[13],
                m[14],
                m[15]);

            matrix4d.ClearProjection();
            matrix4d.ClearRotation();
            matrix4d.ClearScale();
            matrix4d.ClearTranslation();

            // Demo of multiplying matrices. *Static method*
            // OpenTK.Matrix4d.Mult(left, right);
        }

        static void DemoSharpGL(double[] m)
        {
            // Convert array to multidimensional array.
            double[,] ma = {
                                   { m[0], m[1], m[2], m[3] },
                                   { m[4], m[5], m[6], m[7] },
                                   { m[8], m[9], m[10], m[11] },
                                   { m[12], m[13], m[14], m[15] }
                               };

            var matrix = new SharpGL.SceneGraph.Matrix(ma);

            // Demo of multiplying matrices. *Static method*
            // SharpGL.SceneGraph.Matrix.Multiply(left, right);
        }
    }
}

If it were me, once I settled on a solution, I would simply write extension methods over the Solid Edge API to make working with the matrices easier. There are plenty of examples of how to write Solid Edge API extension methods on GitHub (SolidEdge.Community).

Jason Newell
Solutions Architect
www.jasonnewell.net

Re: Matrix methods

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Pinging @AdityaG and @jay_carlton to see if their group can offer any guidance or sample code.

Jason Newell
Solutions Architect
www.jasonnewell.net

Re: Matrix methods

Valued Contributor
Valued Contributor

Since asking the question, I elected to download and wrap a public C# maths library.  I have no difficulty working with matrices, except that there are a lot of methods and I preferred to start with something rather than start with nothing.

 

About these extension methods, my impression is there's nothing magic about them and they are simply useful methods that use the SolidEdge API.

------------------
Alan Baljeu
Owner, Cornerstone Intelligent Software
Developer of custom CAD software

Re: Matrix methods

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Solid Edge uses the computer graphics row major matrix ordering, as opposed to the math's textbook's column major. That means the 16 values are

 xx  xy  xz  0

 yx  yy  yz  0

 xz  zy  zz  0

 tx  ty  tz  1

consisting of a 3x3 rotation matrix and a translation vector.

 

Given a 3D vector (vx, vy, vz) in the 'local' coordinate system, or space as I like to call it, then the premultiplication

(vx vy vz 1) X [xx xy xz 0]

                      [yx yy yz 0]

                      [zx zy zz 0]

                      [tx ty tz 1]

produces the transformed vector. The applies the rotation followed by the translation.

 

The inverse transformation is formed by multiplying the reverse translation, a negation, followed by the reverse rotation, a transpose.

[ 1  0  0 0] X [xx yx zx 0]

[ 0  1  0 0]     [xy yy zy 0]

[ 0  0  1 0]     [xz yz zz 0]

[tx ty tz 1]     [  0   0   0 1]

 

The appropriate methods should be in the maths library.

 

There is a very brief summary on homogeneous math at the beginning of my article on codeproject at

www.codeproject.com/Articles/68243/Heresy-II-Why-D-Homogeneous-Transform-Clip-Projec

 

Re: Matrix methods

Valued Contributor
Valued Contributor

"The appropriate methods should be in the maths library."

 

I grabbed a library and it has appropriate methods.  Did you have something in mind when you said "the maths library"?

------------------
Alan Baljeu
Owner, Cornerstone Intelligent Software
Developer of custom CAD software

Re: Matrix methods

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

No, I had nothing in mind.