Cancel
Showing results for 
Search instead for 
Did you mean: 

Meshing in solid edge API C#

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

I would like to create a nesh in solid edge part with API programming of C#.

Do you know how to proceed ?

 

Thanking you in advance

 

Abdelkader Belhi

4 REPLIES 4

Re: Meshing in solid edge API C#

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Abdelkader,

 

What kind of mesh are looking to create in SE.

Can you describe or post a picture for the same.

 

BR,

Re: Meshing in solid edge API C#

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Tushar,

Thank you for your  answer.

I need only to create a simple part meshing as we do for example in FEMAP in

structural FEM .

is there any object or a class in Solid edge that can do that ?

Thanks

Abdel

Re: Meshing in solid edge API C#

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Abdel,

 

If you are already aware of FEMAP, I've heard it has a full blown API which you can reference in your program. Alas, no API in SE that I know which can mesh. Perhaps @jnewell or someone from the Siemens dev team can answer this.

 

BR,

~Tushar

 

Re: Meshing in solid edge API C#

Siemens Genius Siemens Genius
Siemens Genius

You may want to review the SolidEdge.Part.Interop.StudyOwner and SolidEdge.Part.Interop.Study interfaces.

 

Aditya

---
Aditya Gurushankar
Manager, Solid Edge Planning