Cancel
Showing results for 
Search instead for 
Did you mean: 

Modify Location of balloon text

Pioneer
Pioneer

Hi,

Is there any direct API's for modifying the text location of balloon which is attached to the geometry drawing in draft file?

Currently I am using

Solid Edge FrameworkSupport Type Library > Balloon Object : GetKeyPoint Method for 

getting the location of the text and

Solid Edge FrameworkSupport Type Library > Balloon Object : SetKeyPoint Method

 

for setting the text location of balloon. Also here I am using

Solid Edge FrameworkSupport Type Library > Balloon Object : GetTerminator Method

 

 

to determine whether the balloon is attached to geometry drawing or not.

 

Let me know if you have more details on this.

 

Thanks,

Onkar

2 REPLIES

Re: Modify Location of balloon text

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I was doing some tests and came to the following conclusion:

 

  • Vertex #1 is always the point which was initially clicked during the balloon creation and may not change even if the user drags later the balloon position
  • Additional vertices are only added when using the Alt-Click to add/insert new points on the leader (or via AddVertex/InsertVertex via API)
  • To set the position of the balloon, you should use the SetKeypoint method with the specific KeyPoint indices shown in the image below
  • Keypoint#0 is always identical to the terminator position
  • The terminator object is normally a Reference object to any of the DVLine2d/DVArc2d/... object types

 

ATTENTION: Vertex index starts at 1, but Keypoint index starts at 0 !!

 

I hope this information is helpful to you.

 

Balloons.png

Re: Modify Location of balloon text

Pioneer
Pioneer

Thanks Martin.

 

It will help me while writing codes for modifying location of balloon text.

 

Thanks,

Onkar