Reply

Modify material of multiple parts in assembly mode

[ Edited ]

Hi,

 

I need your help. I need to be able to change the Material of multiple Parts, from within the Assembly

(oApplication.ActiveEnvironment = "Assembly").

 

Right now, to update the Material on the currently opended Part, I call the following function :

 

setProperty(oCurrentPart, "MechanicalModeling", "Material", sProductDesc)

 

... wich is :

 

Private Sub setProperty(ByRef document, ByVal propertySet, ByVal propertyName, ByVal value)

 

Dim oPropertySets As SolidEdgeFramework.PropertySets

 

oPropertySets = document.Properties

 

oPropertySets.Item(propertySet).Item(propertyName).Value = value

 

End Sub

 

Do I need to enter in Part Mode (oApplication.ActiveEnvironment = "Part") for each Part, then use my function (setProperty()) ?

If so, what is the command to enter in part mode from the assembly ?

In pseudo-code : currentAssembly.part("door.par").setActive ... or currentAssembly.openpart("door.par") ...

 

I also need to do the same thing for custom fields, which I currently update with :

setProperty(oCurrentPart, "Custom", "CustomVariable", "CustomValue")

 

Thanks in advance for your help !

 

Jean-Sébastien Jeannotte

 

Posted by: Jean-Sebastien Jeannotte
Post date: 3/30/2007 6:22:22 AM

2 REPLIES

RE: Modify material of multiple parts in assembly mode

[ Edited ]

Hi Jean-Sébastien,

 

you can use the OccurrenceDocument property of an Occurrence instance - SolidEdgeAssembly.AssemblyDocument.Occurrences.Item(n).

 

The OccurrenceDocument can be cast to a SolidEdgeFrameWork.SolidEdgeDocument and from there you can access the properties.

 

Cheers

Calum

 

Posted by: Calum McLellan
Post date: 4/2/2007 1:31:59 AM

RE: Modify material of multiple parts in assembly mode

[ Edited ]

Calum,

 

Can you please provide code snippet for this. i tried it but it is not working for me.

 

Posted by: Prasad Pawar
Post date: 6/11/2008 7:58:16 PM