Cancel
Showing results for 
Search instead for 
Did you mean: 

Modifying 4 chamfers with Visual Basic

Creator
Creator

I'm new to working with SE with Visual Basic and the forum. I have made a part file of a simple tube with 4 sharp edges. I can add chamfer with VB on all the edges. My issue is I need 4 different sized chamfers. I can not see how to change the chamfer with different values. I've worked on this for Day 2 and think it's time ask for some advice.  

 

Thanks in Advance 

 

Dim SE As SolidEdgeFramework.Application
Dim Model As Model
Dim ExtProt As ExtrudedProtrusion
Dim Edgs As Edges
Dim EdgArr(0 To 3) As Edge
Dim Chamfer As SolidEdgePart.Chamfer

SE = GetObject(, "solidedge.application")
Model = SE.ActiveDocument.models.item(1)
ExtProt = Model.ExtrudedProtrusions.Item(1)
Edgs = ExtProt.Edges(EdgeType:=SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll)


EdgArr(0) = Edgs.Item(1)
EdgArr(1) = Edgs.Item(2)
EdgArr(2) = Edgs.Item(3)
EdgArr(3) = Edgs.Item(4)

Chamfer = Model.Chamfers.AddEqualSetback(NumberOfEdgeSets:=4, EdgeSetArray:=EdgArr, SetbackDistance:=0.001)

6 REPLIES

Re: Modifying 4 chamfers with Visual Basic

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi @LenC,

you nees 4 different chamfer objeccts. A Chamfer object the references 4 edges will change all to the same value.

Additional you have to create new chamfer objects if you like to change from equal setback to  one of the other types (see ChamferType value).

You also cannot change the type in the UI of Solid Edge.

If you have a equal setback Chamfer the only  value you can change is ChamferSetbackValue1.

regards

JB
SE ST10

Re: Modifying 4 chamfers with Visual Basic

Creator
Creator

@JB

 

Thank you for the advice.

 

I think I am creating a object correctly but the computer is telling me otherwise. I  error at chamfer1.ChamferSetbackValue1 = 0.001. I Dim and tie Chamfer1 to Chamfers.Item(1). I do not understand am I not creating Chamfer1 correctly. The Chamfer is named chamfer 1  on the model.

 

 

Dim chamfer1 As SolidEdgePart.Chamfer = Nothing

 chamfer1 = model.Chamfers.Item(1)

'chamfer1.ChamferSetbackValue1 = 0.001

Re: Modifying 4 chamfers with Visual Basic

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hi could you share your SE file?
What version of SE are you using?
regards

JB
SE ST10

Re: Modifying 4 chamfers with Visual Basic

Creator
Creator

@JB

 

I'm using ST8. 

Re: Modifying 4 chamfers with Visual Basic

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi, I opened your part.
You have created the chamfers in synchronous mode. So they cannot be modified the way you like.
Change mode to ordered

partDocument.ModellingMode = seModelingModeOrdered

before you add  the chamfers, or even before you create the ring body if you like.

regards

JB
SE ST10

Re: Modifying 4 chamfers with Visual Basic

Creator
Creator
Thanks, That was a big Help