Cancel
Showing results for 
Search instead for 
Did you mean: 

Moving addin created within st8 to st6

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 

I'm using ST8 so I have created an addin  using interop et solidedgecommunity version 108.0.
Now i want to use the same addin in ST6.I'have noticed that there are some modifications in the API.
Like, when i run my addin in st6 , i have for example no member listed for FileMissing() methode attached to the occurance in the assembly.
how can i fix problems related to the API..Is there other API that i have to use??
Any Help would be appriciated.

2 REPLIES

Re: Moving addin created within st8 to st6

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You would need to identify those API elements that do not exist in ST6 and not use them in your code.  There was an ST6 version of the solidedgecommunity that you can download and install from the Nuget site if you prefer. 



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Moving addin created within st8 to st6

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you.