Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Normal cutout on curved surface with wrap sketch using program

Valued Contributor
Valued Contributor

Hi All,

 

I'm trying to do a normal cutout on the surface of a protrusion with a wrap sketch on it through code.

 

I'm trying to use the "Model.NormalCutouts.AddFiniteMulti()" method to do so but everytime it's failing.

 

Can someone suggest me which profile can be passed in case of wrap sketch for the argument in the "AddFiniteMulti" method.

 

Thanks in advance.

 

 

 

1 REPLY

Re: Normal cutout on curved surface with wrap sketch using program

Valued Contributor
Valued Contributor

Hi Guys,

 

I figured it out.

 

So, in case if any of you is ever trying to do a wrap sketch and then do a Normal cutout of it you need to use the:          "NormalToFaceCutouts.Add()" method.

 

And in the arguments for input curves you can pass the array of edges of the wrap sketch present on the surface.

 

Thanks.