Cancel
Showing results for 
Search instead for 
Did you mean: 

Occurrence.MakeWritable - When do you need it?

Valued Contributor
Valued Contributor

 

Hello,

The Occurrence object has MakeWritable method.

When do you need to use it? In other words, how does an occurrence become non-writable? When should we check if the occurrence is writable? Or should we check it every time we want to edit the occurrence?

- Nirantar Vidyarthee

 

Posted by: Narantar Vidyarthee
Post date: 5/29/2010 5:04:56 PM

1 REPLY

RE: Occurrence.MakeWritable - When do you need it?

Valued Contributor
Valued Contributor

How does an occurrence become non-writable? this is a good question!

I have sometimes problems, if i try to change the properties of opened files (occurrences in the opened assemblies).

i check if the occurrenceDocument is writable with objDoc.SeekWriteAccess(glAccess)and if not than i do MakeWritable.

 

Posted by: JR
Post date: 6/7/2010 2:10:49 AM