Cancel
Showing results for 
Search instead for 
Did you mean: 

OpenWithTemplate()

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter

I have a C++ program that manages the full lifecycle of Edge instances. When it has an instance open, I am trying to get it to open ProE assemblies & parts to convert them to SE format (I successfully used an earlier version of this program to convert some old drawings that were in DWG format - I was able to do that using the Open() method).

 

To open these assemblies, I am trying to use the OpenWithTemplate() method.

 

SolidEdgeFramework::DocumentsPtr pDocs = m_pApplication->Documents;

SolidEdgeAssembly::AssemblyDocumentPtr pAssy = pDocs->OpenWithTemplate(_bstr_t(filePath), _bstr_t(_T("G:\\iso assembly.asm")));

 

This causes SE to throw an error about not being able to access the template. The indicated file has normal file attributes and permissions should allow access. I have tried a few ways of passing the template name to it, including a call to

 

SolidEdgeFramework::DocumentTypeConstants docType = SolidEdgeFramework::igAssemblyDocument;

CString tempName = GetTemplateFileName(&docType);

 

But this never returns.

 

Any ideas as to what's causing this behaviour? Cheers.

3 REPLIES 3

Re: OpenWithTemplate()

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Nick,

I believe the specified template has to be just the pure file name of a Solid Edge file in the template folder (I.e. "Normal.par").
Kind regards,
Wolfgang Kunert - www.wksyspro.de

Re: OpenWithTemplate()

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter

That's not what the documentation shows, and not what GetTemplateFileName() returns either (I realised that method pops up the template selection window, but was hidden behind something else so I didn't see it). But even when I use that method as the second argument in OpenWithTemplate(), it still says that the template was not found, couldn't be accessed, etc. I did try with just the plain filename as well though, and no good either.

 

Oddly, I can open an assembly using Open(), but of course it pops up the template selection window still.

Re: OpenWithTemplate()

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter
Both methods work - SE was throwing me off with an innaccurrate error message. Problem was actually down to the name of the file to be opened, and not the template at all!