Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Original Command

Valued Contributor
Valued Contributor

Dear All.

 

I want to make original command, which differ from original

hole command, such as option selection.

 

I think it's not possible to replace hole's option dialog

with user defined dialog.

So I think I have to make full original "Hole" command.

 

In this case, there are several difficulty.

Can someone give idea or sample code for below functions?

 

1) Create ribbon bar

Does someone have sample code for VB.net?

2) On ribbon bar "Hole Plane Step"

This select plane and change to profile environment

and change ribbon bar.

Is it possible to chage profile environment?

3) On ribbon bar "Hole Extension Step"

If I move mouse and model change dynamiccaly,

I think this function is too dificult for me.

 

I'm very glad if someone else help me.

 

Miya

Best regards.

 

Posted by: Hayato Miyato
Post date: 9/20/2006 8:39:52 PM

1 REPLY

RE: Original Command

Valued Contributor
Valued Contributor

Hayato,

 

I wish that I could help you with this one but I'm afraid that I don't know how to do what you're wanting.

 

Does anyone have any suggestions for Hayato?

 

Posted by: Jason Newell
Post date: 9/24/2006 1:31:01 PM