01-18-2015 09:14 PM - edited 01-18-2015 09:16 PM
Hello everyone,
I am glad to present PacEdge - a Pack and Go program for Solid Edge which is open source.
A detailed tutorial on how to build this program from scratch also exists and can be read here.
Using the free source code, you can also build your own version of Pack n Go for Solid Edge.
Here's a preview of version 1.0 of the program:
~Tushar Suradkar
11-27-2018 02:47 PM
I will gain many levels studying your program.Thanks!
I have to incorporate a Pack N Go in one of my applications.