Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Placing draft dimensions

Genius
Genius

This is solid edge so far behind in implementing the ability to dynamically place dimensions in drawing views?  This seems like basic functionality and is pretty good in Inventor.  Do they not see a need?

Bob Reinkemeyer
CAD Integration developer
Martin Sprocket and Gear Inc.
3 REPLIES 3

Re: Placing draft dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@martyman Not sure what you mean... Can you explain or post a video showing what you are referring to?



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Placing draft dimensions

Genius
Genius

I have two drawing views on a draft sheet (see attachment).   I'm looking for a way to dynamically add dimensions (not using retrieve dimensions) and without additional geometry.  Hope this helps.

Bob Reinkemeyer
CAD Integration developer
Martin Sprocket and Gear Inc.

Re: Placing draft dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@martyman Are you talking about automatically applying dimensions/annotations to the views?

 

If so, that can be done using the Relationship Assistant command.

 

EDIT:  This can only be done to 2D geometry, not drawing views...



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com