Cancel
Showing results for 
Search instead for 
Did you mean: 

Predefined faces for constraints

How can i define faces that will be referent for creating constraints when placed in an assembly? Something like the way screws are placed from standard parts.

Regards.

1 REPLY

Re: Predefined faces for constraints

Siemens Phenom Siemens Phenom
Siemens Phenom

There is not a way to simply define faces that are used to create the relationships. Instead, you would need to create relationships on the occurrence that represent how the occurrence is to be placed in the assembly. Then, you can call the CaptureRelationships method on the Assembly.Occurrence object. Using the screw as an example, you could create a mate or planar align for the flat face and an axial align to align the screw in the hole. Then, capture those two relationships for the screw occurrence.