Reply

Printing Draft

[ Edited ]

 

Hi,

 

In my application, I need to print solid edge draft without opening solid edge like the "Batch Print Program". Currently, I use this code  but it very slow to print a draft: 

type = Type.GetTypeFromProgID("SolidEdge.Application");

 

application = (SolidEdgeFramework.Application)

Activator.CreateInstance(type);

 

application.DisplayAlerts = false;

documents = application.Documents;

 

draft = (SolidEdgeDraft.DraftDocument)documents.Open("C:\\test.dft", Missing.Value, Missing.Value, Missing.Value, Missing.Value, Missing.Value);

draft.PrintOut(strDefaultPrinter, 1, 2, System.Drawing.Printing.PaperKind.Standard11x17, 1, false, "", 1, null, true, false);

Does someone have another solution?

Thank

 

Posted by: Patrick Fortier
Post date: 7/3/2009 5:49:06 AM

3 REPLIES

RE: Printing Draft

[ Edited ]

 

HI,

on C:\Program Files\Solid Edge ST\SDK\Readers\DraftDataAPI.doc,

there is a way to extract EMF files from draft documents, without running solidedge.

Seems to be faster. Than you must add code to print EMF files.

regards

Massimo

 

Posted by: Massimo Magris
Post date: 7/3/2009 8:41:50 AM

RE: Printing Draft

[ Edited ]

Dear, Could you tell me how to set PaperSize and PrintRange with C++? Thanks!

 

Posted by: assassin 007
Post date: 7/9/2010 4:43:02 AM

RE: Printing Draft

[ Edited ]

I've Solved the problem.

?? ? ??

DMPAPER_LETTER 1 US Letter 8 1/2 x 11 in

DMPAPER_LETTERSMALL 2 US Letter Small 8 1/2 x 11 in

DMPAPER_TABLOID 3 US Tabloid 11 x 17 in

DMPAPER_LEDGER 4 US Ledger 17 x 11 in

DMPAPER_LEGAL 5 US Legal 8 1/2 x 14 in

DMPAPER_STATEMENT 6 US Statement 5 1/2 x 8 1/2 in

DMPAPER_EXECUTIVE 7 US Executive 7 1/4 x 10 1/2 in

DMPAPER_A3 8 A3 297 x 420 mm

DMPAPER_A4 9 A4 210 x 297 mm

DMPAPER_A4SMALL 10 A4 Small 210 x 297 mm

DMPAPER_A5 11 A5 148 x 210 mm

DMPAPER_B4 12 B4 (JIS) 257 x 364 mm

DMPAPER_B5 13 B5 (JIS) 182 x 257 mm

DMPAPER_FOLIO 14 Folio 8 1/2 x 13 in

DMPAPER_QUARTO 15 Quarto 215 x 275 mm

DMPAPER_10X14 16 10 x 14 in

DMPAPER_11X17 17 11 x 17 in

DMPAPER_NOTE 18 US Note 8 1/2 x 11 in

DMPAPER_ENV_9 19 US Envelope #9 3 7/8 x 8 7/8

DMPAPER_ENV_10 20 US Envelope #10 4 1/8 x 9 1/2

DMPAPER_ENV_11 21 US Envelope #11 4 1/2 x 10 3/8

DMPAPER_ENV_12 22 US Envelope #12 4 3/4 x 11 in

DMPAPER_ENV_14 23 US Envelope #14 5 x 11 1/2

DMPAPER_CSHEET 24 C size sheet

DMPAPER_DSHEET 25 D size sheet

DMPAPER_ESHEET 26 E size sheet

DMPAPER_ENV_DL 27 Envelope DL 110 x 220mm

DMPAPER_ENV_C5 28 Envelope C5 162 x 229 mm

DMPAPER_ENV_C3 29 Envelope C3 324 x 458 mm

DMPAPER_ENV_C4 30 Envelope C4 229 x 324 mm

DMPAPER_ENV_C6 31 Envelope C6 114 x 162 mm

DMPAPER_ENV_C65 32 Envelope C65 114 x 229 mm

DMPAPER_ENV_B4 33 Envelope B4 250 x 353 mm

DMPAPER_ENV_B5 34 Envelope B5 176 x 250 mm

DMPAPER_ENV_B6 35 Envelope B6 176 x 125 mm

DMPAPER_ENV_ITALY 36 Envelope 110 x 230 mm

DMPAPER_ENV_MONARCH 37 US Envelope Monarch 3.875 x 7.5 in

DMPAPER_ENV_PERSONAL 38 6 3/4 US Envelope 3 5/8 x 6 1/2 in

DMPAPER_FANFOLD_US 39 US Std Fanfold 14 7/8 x 11 in

DMPAPER_FANFOLD_STD_GERMAN 40 German Std Fanfold 8 1/2 x 12 in

DMPAPER_FANFOLD_LGL_GERMAN 41 German Legal Fanfold 8 1/2 x 13 in

DMPAPER_ISO_B4 42 B4 (ISO) 250 x 353 mm

DMPAPER_JAPANESE_POSTCARD 43 Japanese Postcard 100 x 148 mm

DMPAPER_9X11 44 9 x 11 in

DMPAPER_10X11 45 10 x 11 in

DMPAPER_15X11 46 15 x 11 in

DMPAPER_ENV_INVITE 47 Envelope Invite 220 x 220 mm

DMPAPER_RESERVED_48 48 RESERVED--DO NOT USE

DMPAPER_RESERVED_49 49 RESERVED--DO NOT USE

DMPAPER_LETTER_EXTRA 50 US Letter Extra 9 1/2 x 12 in

DMPAPER_LEGAL_EXTRA 51 US Legal Extra 9 1/2 x 15 in

DMPAPER_TABLOID_EXTRA 52 US Tabloid Extra 11.69 x 18 in

DMPAPER_A4_EXTRA 53 A4 Extra 9.27 x 12.69 in

DMPAPER_LETTER_TRANSVERSE 54 Letter Transverse 8 1/2 x 11 in

DMPAPER_A4_TRANSVERSE 55 A4 Transverse 210 x 297 mm

DMPAPER_LETTER_EXTRA_TRANSVERSE 56 Letter Extra Transverse 9 1/2 x 12 in

DMPAPER_A_PLUS 57 SuperA/SuperA/A4 227 x 356 mm

DMPAPER_B_PLUS 58 SuperB/SuperB/A3 305 x 487 mm

DMPAPER_LETTER_PLUS 59 US Letter Plus 8.5 x 12.69 in

DMPAPER_A4_PLUS 60 A4 Plus 210 x 330 mm

DMPAPER_A5_TRANSVERSE 61 A5 Transverse 148 x 210 mm

DMPAPER_B5_TRANSVERSE 62 B5 (JIS) Transverse 182 x 257 mm

DMPAPER_A3_EXTRA 63 A3 Extra 322 x 445 mm

DMPAPER_A5_EXTRA 64 A5 Extra 174 x 235 mm

DMPAPER_B5_EXTRA 65 B5 (ISO) Extra 201 x 276 mm

DMPAPER_A2 66 A2 420 x 594 mm

DMPAPER_A3_TRANSVERSE 67 A3 Transverse 297 x 420 mm

DMPAPER_A3_EXTRA_TRANSVERSE 68 A3 Extra Transverse 322 x 445 mm

DMPAPER_DBL_JAPANESE_POSTCARD 69 Japanese Double Postcard 200 x 148 mm

DMPAPER_A6 70 A6 105 x 148 mm

DMPAPER_JENV_KAKU2 71 Japanese Envelope Kaku #2

DMPAPER_JENV_KAKU3 72 Japanese Envelope Kaku #3

DMPAPER_JENV_CHOU3 73 Japanese Envelope Chou #3

DMPAPER_JENV_CHOU4 74 Japanese Envelope Chou #4

DMPAPER_LETTER_ROTATED 75 Letter Rotated 11 x 8 1/2 11 in

DMPAPER_A3_ROTATED 76 A3 Rotated 420 x 297 mm

DMPAPER_A4_ROTATED 77 A4 Rotated 297 x 210 mm

DMPAPER_A5_ROTATED 78 A5 Rotated 210 x 148 mm

DMPAPER_B4_JIS_ROTATED 79 B4 (JIS) Rotated 364 x 257 mm

DMPAPER_B5_JIS_ROTATED 80 B5 (JIS) Rotated 257 x 182 mm

DMPAPER_JAPANESE_POSTCARD_ROTATED 81 Japanese Postcard Rotated 148 x 100 mm

DMPAPER_DBL_JAPANESE_POSTCARD_ROTATED 82 Double Japanese Postcard Rotated 148 x 200 mm

DMPAPER_A6_ROTATED 83 A6 Rotated 148 x 105 mm

DMPAPER_JENV_KAKU2_ROTATED 84 Japanese Envelope Kaku #2 Rotated

DMPAPER_JENV_KAKU3_ROTATED 85 Japanese Envelope Kaku #3 Rotated

DMPAPER_JENV_CHOU3_ROTATED 86 Japanese Envelope Chou #3 Rotated

DMPAPER_JENV_CHOU4_ROTATED 87 Japanese Envelope Chou #4 Rotated

DMPAPER_B6_JIS 88 B6 (JIS) 128 x 182 mm

DMPAPER_B6_JIS_ROTATED 89 B6 (JIS) Rotated 182 x 128 mm

DMPAPER_12X11 90 12 x 11 in

DMPAPER_JENV_YOU4 91 Japanese Envelope You #4

DMPAPER_JENV_YOU4_ROTATED 92 Japanese Envelope You #4 Rotated

DMPAPER_P16K 93 PRC 16K 146 x 215 mm

DMPAPER_P32K 94 PRC 32K 97 x 151 mm

DMPAPER_P32KBIG 95 PRC 32K(Big) 97 x 151 mm

DMPAPER_PENV_1 96 PRC Envelope #1 102 x 165 mm

DMPAPER_PENV_2 97 PRC Envelope #2 102 x 176 mm

DMPAPER_PENV_3 98 PRC Envelope #3 125 x 176 mm

DMPAPER_PENV_4 99 PRC Envelope #4 110 x 208 mm

DMPAPER_PENV_5 100 PRC Envelope #5 110 x 220 mm

DMPAPER_PENV_6 101 PRC Envelope #6 120 x 230 mm

DMPAPER_PENV_7 102 PRC Envelope #7 160 x 230 mm

DMPAPER_PENV_8 103 PRC Envelope #8 120 x 309 mm

DMPAPER_PENV_9 104 PRC Envelope #9 229 x 324 mm

DMPAPER_PENV_10 105 PRC Envelope #10 324 x 458 mm

DMPAPER_P16K_ROTATED 106 PRC 16K Rotated

DMPAPER_P32K_ROTATED 107 PRC 32K Rotated

DMPAPER_P32KBIG_ROTATED 108 PRC 32K(Big) Rotated

DMPAPER_PENV_1_ROTATED 109 PRC Envelope #1 Rotated 165 x 102 mm

DMPAPER_PENV_2_ROTATED 110 PRC Envelope #2 Rotated 176 x 102 mm

DMPAPER_PENV_3_ROTATED 111 PRC Envelope #3 Rotated 176 x 125 mm

DMPAPER_PENV_4_ROTATED 112 PRC Envelope #4 Rotated 208 x 110 mm

DMPAPER_PENV_5_ROTATED 113 PRC Envelope #5 Rotated 220 x 110 mm

DMPAPER_PENV_6_ROTATED 114 PRC Envelope #6 Rotated 230 x 120 mm

DMPAPER_PENV_7_ROTATED 115 PRC Envelope #7 Rotated 230 x 160 mm

DMPAPER_PENV_8_ROTATED 116 PRC Envelope #8 Rotated 309 x 120 mm

DMPAPER_PENV_9_ROTATED 117 PRC Envelope #9 Rotated 324 x 229 mm

DMPAPER_PENV_10_ROTATED 118 PRC Envelope #10 Rotated 458 x 324 mm

 

 

Posted by: assassin 007
Post date: 7/12/2010 9:34:21 PM