Cancel
Showing results for 
Search instead for 
Did you mean: 

Propseed file

Valued Contributor
Valued Contributor

I have this macro that will link to the propseed file but I want the macro to remember at load time where it is located and have the option to seth a new path (via a FolderBrowserDialog) if the file gets moved.

What would be the simplest way, use registry keys?

 

Posted by: Yoland Gagnon
Post date: 1/10/2006 6:37:25 AM

5 REPLIES

RE: Propseed file

Valued Contributor
Valued Contributor

Yoland,

 

I usually have a Settings class with static (shared in VB.NET) methods that I can call from anywhere in my code to save settings. For example: Settings.SetPropseedPath(path as string)

 

 

Posted by: Jason Newell
Post date: 1/10/2006 8:55:12 AM

RE: Propseed file

Valued Contributor
Valued Contributor

My macro (exe) will be distributed though to 10 users, you wouldn't have an example of what you are doing (Settings class) and how you relate to it? Thanks :-)

 

Posted by: Yoland Gagnon
Post date: 1/13/2006 1:06:54 AM

RE: Propseed file

Valued Contributor
Valued Contributor

Ok I figured out how to do it using SaveSetting & GetSetting. It does what I wanted, thanks Jason

I am trying to find an example of how to retrieve data from the propseed file, do you have any example at hand?

Thanks in advance for your help.

 

 

 

Posted by: Yoland Gagnon
Post date: 1/16/2006 5:27:58 AM

RE: Propseed file

Valued Contributor
Valued Contributor

Yoland,

 

I have written a class called PropseedParser but I cannot share it as it was written for a customer.

 

I can give you hints on how to create your own though.

 

You'll need to analyze the format of the file.

 

- Notice that lines with "\\" are remarks.

- Notice that standard properties have Begin \ End blocks.

- Notice that custom properties have Begin Define Custom block and then corresponding Begin \ End blocks.

 

You can use File.OpenText() to open a StreamReader with allows you to iterate through the lines.

 

Good luck

 

Posted by: Jason Newell
Post date: 1/16/2006 5:59:36 AM

RE: Propseed file

Valued Contributor
Valued Contributor

Cool, thanks Jason, I'll start from that.

Have a nice day

 

Posted by: Yoland Gagnon
Post date: 1/16/2006 6:48:52 AM