Cancel
Showing results for 
Search instead for 
Did you mean: 

Range + 6.35 mm

Gears Phenom Gears Phenom
Gears Phenom

I noticed this and hence want to confirm if it's true that the Range method returns 6.35 mm added to the actual coordinates:

Here's a DrawingView of a 100 mm x 100 mm cube placed at the origin with its cropping box:

 

range2.png

The Range method on this DrawingView returns 100 + 6.35 mm

 

debugrange.png

 

I want to know why it doesn't return just 100 x 100 or how can the setting be changed in SE so that the cropping border fits tightly to the actual extents of the DrawingView and the Range method returns the exact values.

 

Another example:

range.png

 

Any insight is highly appreciated:

 

~Tushar

 

2 REPLIES

Re: Range + 6.35 mm

Phenom
Phenom

I suspect it would cause problems with processing lines that lay along the view border - as the edges of your cube would be.

Are they inside or outside the border?

 

Someone has decided that 6.35mm (1/4") is a reasonable amount.

 

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Range + 6.35 mm

Gears Phenom Gears Phenom
Gears Phenom

Thanks @beachcomber  for confirming this.

related question has been posted by @hawcad

 

~Tushar