Cancel
Showing results for 
Search instead for 
Did you mean: 

Retriving Custom Properties of an assembly occurence

Valued Contributor
Valued Contributor

 

Hi all

I am new to Solid Egde Programming and to this community. I want to retrive the properties under the "Custom" Tab of Document File Properties through VB?

I will be grate to recieve the any help in this regards.

Thanks In Advance

Regards                                                                                                       

Noman Syed

 

Posted by: Noman Syed
Post date: 11/14/2007 1:10:10 AM

2 REPLIES

RE: Retriving Custom Properties of an assembly occurence

Valued Contributor
Valued Contributor

 

Noman,

See the following code and attachment.

 Imports SolidEdgeAssemblyImports SolidEdgeFrameworkImports System.Runtime.InteropServicesModule Module1 Sub Main() Dim objApp As SolidEdgeFramework.Application Dim objAssembly As SolidEdgeAssembly.AssemblyDocument Dim objOccurrences As SolidEdgeAssembly.Occurrences Dim objOccurrence As SolidEdgeAssembly.Occurrence objApp = Marshal.GetActiveObject("SolidEdge.Application") 'I used "C:\Program Files\Solid Edge V20\Training\Coffee Pot.asm" objAssembly = objApp.ActiveDocument objOccurrences = objAssembly.Occurrences For Each objOccurrence In objOccurrences ProcessOccurrence(objOccurrence) Next End Sub Sub ProcessOccurrence(ByVal objOccurrence As SolidEdgeAssembly.Occurrence) Dim objSubOccurrences As SolidEdgeAssembly.SubOccurrences = Nothing Dim objSubOccurrence As SolidEdgeAssembly.SubOccurrence = Nothing Try ' 1st level of an assembly are of type SolidEdgeAssembly.Occurrence. GetDocumentCustomProperty(objOccurrence.OccurrenceDocument, "CUSTOM NAME FIELD") ' 2st level and lower of an assembly are of type SolidEdgeAssembly.SubOccurrence. objSubOccurrences = objOccurrence.SubOccurrences If Not (objSubOccurrences Is Nothing) Then For Each objSubOccurrence In objSubOccurrences 'Recursive call to walk the assembly tree ProcessSubOccurrenceSubOccurrences(objSubOccurrence) Next End If Catch ex As Exception Console.WriteLine(ex.Message) End Try End Sub Sub ProcessSubOccurrenceSubOccurrences(ByVal objSubOccurrence As SolidEdgeAssembly.SubOccurrence) Dim objSubOccurrenceSubOccurrences As SolidEdgeAssembly.SubOccurrences = Nothing Dim objSubOccurrenceSubOccurrence As SolidEdgeAssembly.SubOccurrence = Nothing GetDocumentCustomProperty(objSubOccurrence.SubOccurrenceDocument, "CUSTOM NAME FIELD") objSubOccurrenceSubOccurrences = objSubOccurrence.SubOccurrences If Not (objSubOccurrenceSubOccurrences Is Nothing) Then For Each objSubOccurrenceSubOccurrence In objSubOccurrenceSubOccurrences GetDocumentCustomProperty(objSubOccurrenceSubOccurrence.SubOccurrenceDocument, "CUSTOM NAME FIELD") Next End If End Sub Sub GetDocumentCustomProperty(ByVal objDocument As SolidEdgeFramework.SolidEdgeDocument, ByVal propertyName As String) Dim objPropertySets As SolidEdgeFramework.PropertySets = Nothing Dim objProperties As SolidEdgeFramework.Properties = Nothing Dim objProperty As SolidEdgeFramework.Property = Nothing Try objPropertySets = objDocument.Properties objProperties = objPropertySets.Item("Custom") objProperty = objProperties.Item(propertyName) Console.WriteLine(String.Format("{0}: {1} = {2}", objDocument.Name, propertyName, objProperty.Value.ToString())) Catch ex As Exception Console.WriteLine(ex.Message) End Try End SubEnd Module

 

Posted by: Jason Newell
Post date: 11/18/2007 8:29:29 PM

RE: Retriving Custom Properties of an assembly occurence

Valued Contributor
Valued Contributor

 

Jason:

Thank you very much

Regards

Noman Syed

 

Posted by: Noman Syed
Post date: 11/21/2007 3:37:44 AM