Cancel
Showing results for 
Search instead for 
Did you mean: 

RevisionManager.SetActionInRevisionManager

Valued Contributor
Valued Contributor

Dear All,

 

I'm trying to work with the function SetActionInRevisionManager of the revision manager class.

 

Its arguments are: SetActionInRevisionManager(nFileCount As Integer, ListOfInputFileNames As Object, ListOfInputActions As Object, Optional ListOfNewFileNames As Object = Nothing, Optional NewFilePathForAllFiles As Object = Nothing)

 

What i want my program to do is to open the revision manager, let it open an assembly and let it rename every occurence wich has a filename containing xx-xxxx to a drawing number like 99-9999.

 

I'm able to programatically open the revision manager and open the assembly in the manager with vb.net. the only thing i can't seem to get working is this SetActionInRevisionManager function.

 I create three lists:

RenameList:list of strings containing all fileNames i want to rename
RenameAction: list of same size with each element:

= RevisionManager.RevisionManagerAction.RenameAction

RenameToList: list of same size with all new file names

Directory: path of the directory.

 

Then i call

 

objRevisionManager.SetActionInRevisionManager(RenameList.Count, RenameList, RenameAction, directory)
It doesn't give me an error but nothing changes in the revision manager.

Am i using this function wrongly?
Thanks for your help.

Kr,

 

4 REPLIES

Re: RevisionManager.SetActionInRevisionManager

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I created PerformRenameAction sample for you on GitHub.

Jason Newell
Applications Architect
www.jasonnewell.net

Re: RevisionManager.SetActionInRevisionManager

Valued Contributor
Valued Contributor
Thanks for your reply Jason.
Unfortunatly i'm working on an urgent project at the moment.
But i'm sure i'll find your example usefull.

I'll let you know when i got my program to work.
Kind Regards,
Vandewaerde David

Re: RevisionManager.SetActionInRevisionManager

Phenom
Phenom

I used this sample as the basis for a very useful application for our company to post-process the file names of a Teamcenter assembly export before sending to our fabricators.  It had to be done manually before so thanks a lot for the help!

Re: RevisionManager.SetActionInRevisionManager

Valued Contributor
Valued Contributor

Hi Jason,

Thanks a bunch,

I finay got it working.
So the arguments should be inserted as an array instead as a List Smiley Happy

 

Don't you agree it is a little confussing defining the function as following:

Function SetActionInRevisionManager(nFileCount As Integer, ListOfInputFileNames As Object, ListOfInputActions As Object, Optional ListOfNewFileNames As Object = Nothing, Optional NewFilePathForAllFiles As Object = Nothing)

ListOfInputFileNames

ListOfInputActions

ListOfNewFileNames

while in fact they should be are arrays instead of lists? Smiley Happy

 Ps: if you were to visit Belgium one day, remind me to buy you a drink!
You've been helping me out quite some times here and i really appreciate it!

 

Thanks a bunch!