Cancel
Showing results for 
Search instead for 
Did you mean: 

SE 2019 won't load silent docs

Experimenter
Experimenter

I can get drafts to open silently, although its a little wonky, but assemblies and parts always open with a ui - 

 

 

Dim oASM as AsssemblyDocument = oDOCS.Open(AsmPath, 8)

Dim oPAR as PartDocument = oDOCS.Open(ParPath, 8)

 

Am I misunderstanding something or is this "feature" just not working?

 

Thanks in advance.

3 REPLIES 3

Re: SE 2019 won't load silent docs

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I think it should be working. 

I learnt about that option years ago and didn't test it much.

Today I found a thread in this forum fom Jason Newell referring to this blog post talking about opening files silently.

Very interesting.

Maybe you can get some answers there...

 

Julian Guillo
Pixel Sistemas SL
Spain

Re: SE 2019 won't load silent docs

Experimenter
Experimenter

Thats exactly where I was looking originally. It seems like it only works (barely) for drafts now, parts and assemblies still open visibly regardless of the extra "8"

 

On MP4 if it makes a difference at all.

Re: SE 2019 won't load silent docs

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I am traveling this week so I'm not at my normal dev machine with 2019. When I get back, I will do some testing and see what results I get and report back.

 

Regarding the mentioned blog post and ensuing conversations, it's one of my all time favorite. Such a good discussion. Someone needs to follow up on that IR. <-- Me

 

Hacks are fun. Until they break. Then they're not fun anymore.

Jason Newell
Solutions Architect
www.jasonnewell.net