Cancel
Showing results for 
Search instead for 
Did you mean: 

SE ST crashes on application.quit()

Valued Contributor
Valued Contributor

 

Hi there,

once upon a time I wrote an app in C# for SE19, which has worked flawlessly.

Now trying the same app with SE ST, the program makes ST sometimes crash at the line:

applicationObject.Quit();

The message is: .NET BroadcastEventWindow.2.0.0.0.33c0d9d.0 Edge.exe

With SE19 everything is fine. Does anybody have an idea where to start looking for the error?

thanks,

Sibi

 

Posted by: Seb Sosna
Post date: 11/4/2008 1:43:51 AM

1 REPLY 1

RE: SE ST crashes on application.quit()

Valued Contributor
Valued Contributor

Ok I found out.

 

SE ST (100) is picky about the registry. I've manipulated a value in the addins and set it to 0 during program execution. SE 19 doesn't care about it, but SE ST expects 0X000000...

 

Sibi

 

Posted by: Seb Sosna
Post date: 11/6/2008 5:20:36 AM