Cancel
Showing results for 
Search instead for 
Did you mean: 

SE-file-properties in Explorer (file manager)

Valued Contributor
Valued Contributor

I seem to remember that it's possible to change the appearance of Windows Explorer (file manager) to show SE properties. Now only the "standard" properties, such as 'title', 'subject', ... are visible in columns. While a lot more properties are available when you go into customizing your explorer view, only a few of them are specific to SE.

 

So is it possible to add them to this list with some kind of registry hack ?

 

Alex

 

Posted by: Alex Haerens
Post date: 1/21/2007 9:33:31 PM

1 REPLY

RE: SE-file-properties in Explorer (file manager)

Valued Contributor
Valued Contributor

Alex,

 

See the Forums -> JasonNewell.NET -> Solid Edge PowerToys threads.

 

This can only be done with a Windows Shell extension. I've been working really hard on it and I'm hoping to get a beta build out this week.

 

Posted by: Jason Newell
Post date: 1/22/2007 1:07:01 AM