Cancel
Showing results for 
Search instead for 
Did you mean: 

SE v20 to SE ST

Valued Contributor
Valued Contributor

 

Hi All,

I use SE v20 and VB.Net to automate the solid edge stuff. Now we are planning to shift to SE ST.

I just want to concern few things that the utilities (automation) we are using right now run on SE v20 & vb.net. Once we change the SE v20 to SE ST, will these utilities get affected?

Or do we need to make some drastic changes in the programming?

Thanks in advance.

 

Posted by: Prasad Pawar
Post date: 10/14/2008 11:07:20 PM

1 REPLY

RE: SE v20 to SE ST

Valued Contributor
Valued Contributor

 

I had the same question but i contacted a supplier of solid edge in the Netherlands and he said it was not a problem. The functions are the same as Solid Edge V20. Also he said there are more functionalities in the ST . 

He tested his own program in ST and had no problems what so ever.

Kind regargds,

Matthijs ter Stege

 

Posted by: Matthijs Stege
Post date: 10/15/2008 12:43:14 AM