Reply

SEMCtl.ocx error

[ Edited ]

 

Hello all,

I am building a program in visual 2008 for solid edge but now i have a big big problem. When I want to add the reference SEMctl.ocx it's not in the com list, when i browse for the reference i get the error:

A reference to 'C:\program files\solid edge v20\program\SEMCtl.ocx' could not be addded. Please make sure that the file is accesible, and that it is a valid assembly or COM component.

I have solid edge not running during this time so that is not the problem.

Please help

Thanks

Matthijs ter Stege

 

Posted by: Matthijs Stege
Post date: 10/10/2008 3:14:47 AM

2 REPLIES

RE: SEMCtl.ocx error

[ Edited ]

Hi,

 

works without a problem here. With VS2008 and SE19. Try to reinstall VS2008 and/or SE.

 

regards,

Sibi

 

Posted by: Seb Sosna
Post date: 10/10/2008 4:12:07 AM

RE: SEMCtl.ocx error

[ Edited ]

Hello Sibster,

 

I work with solid edge v20 and tried to reinstall both programs but it didnt help. I will try it with solid edge ST. Other OCX files of solid edge can be imported but not this one. If it works with solid edge ST i will reply again.

 

Thanks for your help,

Matthijs

 

Posted by: Matthijs Stege
Post date: 10/13/2008 10:45:45 PM