Cancel
Showing results for 
Search instead for 
Did you mean: 

Save as Flat DXF

Valued Contributor
Valued Contributor

Hi

 

I have a small problem in solid edge program ,

 

I want to create the .psm into Dxf file with user selected edge and face and also select the "use Folded model " option in sheet metal properties window in program

 

 

with regards

Srinivas Ande

 

Posted by: Srinivas ande
Post date: 6/9/2012 2:22:23 AM

2 REPLIES

Re: Save as Flat DXF

Valued Contributor
Valued Contributor

in ST3 - while you are in psm environment you can use the "save as flat" from the head menu. if flatten pattern exist it saves as dxf, if not it prompt for selecting face and edge.

 

why do you need a separate program to do this?

 

Posted by: alon raviv
Post date: 6/10/2012 5:06:43 PM

Re: Save as Flat DXF

Valued Contributor
Valued Contributor

Alon Raviv,

 

Thank you for the prompt reply.

 

Manually we are selecting the face and edge to convert the dxf files.

 

We have a small code in vb .net, its converts .psm to .dxf by using "saveasflatdxf" method. it is generates dxf file but my problem is its taking the default orientation.

 

Here i want a single click dxf conversion, because we are converting the number of files, so that its consuming more time. To save this time process we need create add-inn. We need the user required orientation .dxf file by selecting the user.

 

Thanks & Regards.

Srinivas Ande

 

Posted by: Srinivas ande
Post date: 6/11/2012 2:54:35 AM