Saveas is not working if solidedge visibility is set as false

Valued Contributor
Valued Contributor

Hi,

  I am using a function "Saveas" in (C# language) to create Pdf's. This is working if SolidEdge visibility is set as true,whereas if the visibility is set as false then it is throwing an error "File Translation error". So is there any option so that i can use "Saveas" even if visibility is set as false.

 

Thanks

Venkata Ramesh V

 

Posted by: Venkata Ramesh Virodhula
Post date: 7/26/2011 3:19:06 AM

2 REPLIES

RE: Saveas is not working if solidedge visibility is set as false

Valued Contributor
Valued Contributor

Unfortunately it sounds like something that will need to be submitted to GTAC. I too have seen APIs in the past that don't work correctly if the GUI is not visible. If you submit an IR, they may be able to fix it.

 

Posted by: Jason Newell
Post date: 7/26/2011 9:27:05 PM

RE: Saveas is not working if solidedge visibility is set as false

Valued Contributor
Valued Contributor

Thanks jason for the information and i dont know this GTAC and IR. but implementing this is a good thing, i hope. So if possible submit that "IR" and get it solved.

 

(I struggled 4 days reading all the API's for this problem, since i cannot take it granted that things are wrong from tool side..Lot of relief )

 

Thanks again,

Venkata Ramesh V

 

Posted by: Venkata Ramesh Virodhula
Post date: 7/27/2011 1:50:33 AM