Cancel
Showing results for 
Search instead for 
Did you mean: 

Saving Draft Document as Image

Valued Contributor
Valued Contributor

Hello,

 

In Solid Edge ST2, there is command that allows me to save my current sheet in a draft document as an image. This can be done interactively using the Save As->Save As Image command.

 

Is there a way I can do this programmatically? If so, what is the proper function to call?

 

Thanks,

 

Brian

 

Posted by: Brian Mansfield
Post date: 5/17/2012 1:28:52 PM

2 REPLIES

Re: Saving Draft Document as Image

Valued Contributor
Valued Contributor

Brian,

 

you may use the SaveAsImage method of a View object:

 

seApp.Windows(1).View.SaveAsImage(...)

 

with seApp referencing the Solid Edge Application object and Windows(1) being the Window with the contents to be saved as image.

 

Posted by: Wolfgang Kunert
Post date: 5/18/2012 9:23:11 AM

Re: Saving Draft Document as Image

Valued Contributor
Valued Contributor

Brian,

I use next to save every sheet in .dft sa .emf

 

.... Sh := SEDraft.Sheets.Item(i);

... Sh.CopyEMFToClipboard();

 

Georgi

 

Posted by: Georgi Georgiev
Post date: 7/18/2012 7:37:13 AM