Reply

Saving user defined settings in ST7

My company is currently upgrading from ST5 to ST7 and we would like to have Solidedge open to each user with specific options (relationship colors, base reference plans and ordered) turned on. Is there a way to achieve this? I have tested setting the ANSI inch part template to the desired setting and saving it, then when we install and open ST7 on other work center and replace the original ANSI inch part with the modified template is reverted back to the default settings. It seems like Siemens doesn't make it very easy for users to save user defined settings.  Any help would be greatly appreciated.

1 REPLY

Re: Saving user defined settings in ST7

[ Edited ]

Hi,

 

Have a look at the %AppData%\Unigraphics Solutions\Solid Edge folder the customization is save there.

 

In ST7 this will save the Odered or Synchronous choice and other options available in the Customize window you can access with right click on the ribon.

 

Base reference plans are saved in the model document and the relationship color (if you mean change of color of the profil when constrain) is accessible in registry :

[HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 107\PrefSets\Options-Color] "ColorByDOF"=hex:06,00,00,00,00,00,00,00,01,00,00,00,00,00,00,00

 

To find the correct registry key you can use soft that compare 2 shots of the registry base like Regshot.

 

You just have to configure a first workstation in ST7 then copy the different file from this to the others.

 

Also Have a look at SEAdmin that will help you the define some of the option during installation.

 

Romuald.


Romuald BERTIN