Cancel
Showing results for 
Search instead for 
Did you mean: 

Scaling the Drawing View

Valued Contributor
Valued Contributor

 

HI,

   OK here is the problem. I need to scale a view. But when I scale the view the dimensions and annotations do not scale with view. I have set the boolean property "ScaleDimensionANDAnnotations" to true.

   I tried Increasing the text size if the sheet but then, all text overlap each other. I have to scale the view upto 50 times. I need to the maintain the distance between the Dimensions so the they look good.

is there solution for maintaining distance between dimensions so than they don't overlap.

I tried giving track distance also.

Please help........

 

Posted by: Pritam Dulam
Post date: 11/13/2009 9:17:47 PM

1 REPLY

RE: Scaling the Drawing View

Valued Contributor
Valued Contributor

 

Hi,

 

the option "ScaleDimensionANDAnnotations" is only for dimensions placed in DrawingViewEdit.

 

Regards

JR

 

Posted by: JR
Post date: 11/19/2009 1:32:49 AM