Cancel
Showing results for 
Search instead for 
Did you mean: 

Set Active Draft Sheet's Background

I've seached prior post's and can't figure this out...

I knowo this has got to be just a single call that I cant seem to get right...

 

Any help is much appreaciated!!!

 

I know the name of my background sheet.

I know my active sheet.

 

I want to set my active sheet’s background…

 

Can anyone help me out here?

 

Dim objApp As SolidEdgeFramework.Application = Nothing

objApp = Marshal.GetActiveObject("Solidedge.Application") 'try to connect to running instance of SE

 

Dim objWorkingDft As SolidEdgeDraft.DraftDocument = Nothing

objWorkingDft = objApp.ActiveDocument

 

Dim objBackground As SolidEdgeDraft.Sheet

objBackground = objWorkingDft.Sections.Item("Backgrounds").Sheets.Item("PAC_B_Wide")

 

'here I need to set "objWorkingDft"'s background to "objBackground"

'Same as manual UI RMB on sheet tab - sheet set up, Background tab - then select background sheet, check on SHow Background

 

??? Stumped!!!

5 REPLIES

Re: Set Active Draft Sheet's Background

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

objWorkingDft.ActiveSheet.Background = objBackground

 

Kind regards,
Wolfgang Kunert - www.wksyspro.de

Re: Set Active Draft Sheet's Background

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
additional the the sheet size must be set:
objWorkingDft.ActiveSheet.SheetSetup.SheetSizeOption = objBackground.SheetSetup.SheetSizeOption
regards

JB
SE ST10

Re: Set Active Draft Sheet's Background

thanks much!!!   i knew it was just 1 line of code but for the life of me couldnt seem to get it right!

Re: Set Active Draft Sheet's Background

Thanks JB,  Im setting sheet size earlier in my code when im pasting it in....  Had that...  just couldnt figure out how to turn on the background sheet.

 

thanks much!

Re: Set Active Draft Sheet's Background

just to document this for the sake of all and future searches.

 

=================================================

Option Explicit On

 

'The following code sample shows how you can select and set a sheet size

'and a background using VB automation

 

Module Module1

 

    Sub Main()

        Dim App As SolidEdgeFramework.Application

        Dim Doc As SolidEdgeDraft.DraftDocument

        Dim ActiveSheet As SolidEdgeDraft.Sheet

        Dim Section As SolidEdgeDraft.Section

        Dim BackgroundSection As SolidEdgeDraft.Section

        Dim ForegroundSection As SolidEdgeDraft.Section

        Dim WorkingSheet As SolidEdgeDraft.Sheet

 

        Dim I As Integer

        Dim SheetName As String

 

        App = GetObject(, "SolidEdge.Application")

        Doc = App.ActiveDocument

        ActiveSheet = Doc.ActiveSheet

 

        'Set the sheet size

        ActiveSheet.SheetSetup.SheetSizeOption = SolidEdgeDraft.PaperSizeConstants.igAnsiAWide

 

        'Set the corresponding background

        ActiveSheet.Background = Doc.Sections.BackgroundSection.Sheets.Item("A-Sheet")

 

 

        End

 

    End Sub

 

End Module

======================================================================