Cancel
Showing results for 
Search instead for 
Did you mean: 

Set Path in Part Library

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Is there a way to set i.e. change the folder in the Parts Library in the assembly environment ? Thanks.

 

asmPLQ.png

 

~Tushar

 

3 REPLIES

Re: Set Path in Part Library

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If there is a way, I sure don't see it Tushar. I'd suggest an IR and ask GTAC.

Jason Newell
Applications Architect
www.jasonnewell.net

Re: Set Path in Part Library

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Tushar,

 

the path to the parts library gets saved in the user registry under (i.e. ST7):

 

HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 107\Library in the key named PartsLibraryFolder

 

I didn't investigate so far how to get Solid Edge updated without restarting it.

 

 

 

Kind regards,
Wolfgang Kunert - www.wksyspro.de

Re: Set Path in Part Library

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thanks Wolfgang. That was very close.

I tried with creating a new assembly but that does not seem to be the point in time when SE reads the registry for the Library path. Also as you said there is no way in sight to get SE updated without rebooting.

   

This was required in context of this macro where I resorted to use the 'Windows Explorer' to open the path intead of the Part Library of SE.

 

~Tushar