SetFilePropertiesOnServer

Valued Contributor
Valued Contributor

Hello,

has anyone expierience with this function?

I want to change the "Kommentare"-property on server. This property is also a Windows-fileproperty. When I set this property it is written to a temporary property in the SE-properties. This temporary property is written to the windows-property during checking in, but I donot have checked it out. Because this I wnt to try to use SetFilePropertiesOnServer to write the propety to the windows-property at once, but I have no idea how the parameters have to be filled and didnot find any information in the net.

Thanks for your comments

 

Posted by: Andreas Baumann
Post date: 1/29/2013 12:11:48 AM