Cancel
Showing results for 
Search instead for 
Did you mean: 

Setting a variable text

Experimenter
Experimenter

Hello,

 

I have a typical file, which I copy every time and make changes on it.

In order to tell apart each copy, I want to mark every part with its own marking. This marking needs to be physical - that means a serial number on the metal, which will be cutouted afterwards.

 

I don't want to do it manually by SolidWorks for each file, and I understand there's no way to edit text sketch through the API.

What other options are possible for this kind of task?

 

The best way would be - creating a text in SolidEdge - setting it as any variable (I couldn't find such option), and programattically change the variable for every file, in order to change the text. Is that possible?

 

Thanks.

3 REPLIES 3

Re: Setting a variable text

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

There is no way to do that AFAIK.

 

You should open an IR to allow the use of property texts inside a Text profile, just like in Callouts.

 

Regards,

Julian

Julian Guillo
Pixel Sistemas SL
Spain

Re: Setting a variable text

Experimenter
Experimenter

I'm sorry, but what's IR?

can I get more details?

Re: Setting a variable text

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

IR = Incident Report

 

You can submit an IR via GTAC or your VAR.

Jason Newell
Solutions Architect
www.jasonnewell.net