Cancel
Showing results for 
Search instead for 
Did you mean: 

Simplest way to determine if a sheet exists

PLM World Member Genius PLM World Member Genius
PLM World Member Genius

I am writing a function that will replace the background on a sheet with a sheet from another file.  The input parameters include the sheetnames of the source and target.

 

What is the simplest way to determine if a sheet exists in a Draft file?

 

I know I could loop through the sheets collection and return a  boolean if I do find it.  But is there a way to try accessing the sheet by name and just see if an exception comes back?

Dim sourceBackground As SolidEdgeDraft.Sheet 
sourceBackground = oSourceDoc.Sheets.Item(sourceSheetName)

What exception would be thrown in this case if the sheet does not exist?

 

Thanks.

Carl Breving

1 REPLY

Re: Simplest way to determine if a sheet exists

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You are correct Carl. Most if not all Item() methods allow you to pass in a VARIANT (Object). Typically, they're looking for an Integer to specify an index or String to specify a key. I believe in the case of Sheets, each sheet name is used as the key. Regarding which exception is thrown, I believe it's something along of the lines of invalid index.

Jason Newell
Applications Architect
www.jasonnewell.net