Showing results for 
Search instead for 
Did you mean: 

Solid Edge Add-ins

Valued Contributor
Valued Contributor

Hello all,


I have been struggling to create an add-in connected to Solid Edge, but no success.

I have read the posts, try the sample that comes with SE, did the step-by-step from chapter 12 (doc by Siemens) but still no luck.


Is there someone out there, willing to share the code just to connect to Solid Edge, like a base template?

I want to connect with SE ST4/64 bits on Win 7/64 bits, using VB.Net.


In Visual Studio 2010 in debug mode, it is not clear if I have to register the dll when I press F5.

Is this registration only needed whene the app is compiled?


Attached a text file that contains my code to connect.



ANy help would be appreciated.


Thanks a bunch


Marc Stringer


Posted by: Marc Stringer
Post date: 5/14/2012 3:48:09 PM


Re: Solid Edge Add-ins

Valued Contributor
Valued Contributor

May be my answer given in the thread below will help you:


Posted by: Wolfgang Kunert
Post date: 5/23/2012 4:17:49 AM