Solid Edge Addin Wizard for Visual C++ 2008

Valued Contributor
Valued Contributor

 

All,

I have updated the installer for my addin wizard (C++) to work with Visual Studio 2008.  I have not revisited the actual code that the wizard produces so you may have to deal a few issues.  I tried it on my machine and it compiled and executed seemingly ok.

You can find the updated download in Downloads -> Solid Edge Addin Wizard (you must be logged in).

 

Posted by: Jason Newell
Post date: 9/7/2010 11:43:12 PM

7 REPLIES

RE: Solid Edge Addin Wizard for Visual C++ 2008

Valued Contributor
Valued Contributor

 

I tried to create a project using this macro, and I get errors. The first one is "Automation server can't create object" then I get an empty message box. Is there any requirements to use the macro?

Nevermind. Last week something uninstalled every application off of my system (rogue uninstaller of a beta project) and I hadn't reinstalled Solidedge yet.

 

Posted by: Raymond Sanders
Post date: 9/22/2010 4:45:25 AM

RE: Solid Edge Addin Wizard for Visual C++ 2008

Valued Contributor
Valued Contributor

That would do it for sure. The wizard uses the SEInstallData API to determine the path to the Solid Edge type libraries. You do bring up a good point though in that the wizard could handle the error better. Thanks for the feedback.

 

Posted by: Jason Newell
Post date: 9/22/2010 5:21:47 AM

RE: Solid Edge Addin Wizard for Visual C++ 2008

Valued Contributor
Valued Contributor

Hi Jason Newell

I create a addin using this addin wizard, when I build a debug version, all is right, but when I build a release version, the buttons of this add can't use, I dont't know this is why, can you help me? thanks.

 

Posted by: Jason Wang
Post date: 9/28/2010 11:02:41 PM

RE: Solid Edge Addin Wizard for Visual C++ 2008

Valued Contributor
Valued Contributor

 

There is a bug in the code that gets generated.  It is the only bug that I am aware of to date and only appears in Release builds.  Open EventManager.h and navigate to the CEventHandlerBase class.

ChangeHRESULT Connect(IUnknown* pUnk) { HRESULT hr; assert(SUCCEEDED(hr = AtlAdvise(pUnk, this, *piidEvents, &m_dwAdvise))); return hr; }

HRESULT Disconnect(IUnknown* pUnk) { HRESULT hr; assert(SUCCEEDED(hr = AtlUnadvise(pUnk, *piidEvents, m_dwAdvise))); return hr; }

toHRESULT Connect(IUnknown* pUnk) { HRESULT hr = AtlAdvise(pUnk, this, *piidEvents, &m_dwAdvise); return hr; }

HRESULT Disconnect(IUnknown* pUnk) { HRESULT hr = AtlUnadvise(pUnk, *piidEvents, m_dwAdvise); return hr; }

Sorry for the trouble.

 

Posted by: Jason Newell
Post date: 9/29/2010 7:48:51 AM

RE: Solid Edge Addin Wizard for Visual C++ 2008

Valued Contributor
Valued Contributor

Thank you very much! All is OK when I modified.

 

Posted by: Jason Wang
Post date: 9/29/2010 4:00:48 PM

RE: Solid Edge Addin Wizard for Visual C++ 2008

Valued Contributor
Valued Contributor

Hello Jason,

 

I can't see the it in "Downloads -> Solid Edge Addin Wizard". Under "Downloads" folder, there are only "Solid Edge Spy" and "PowerToys for Solid Edge". What's wrong? Thanks in advance.

 

Best regards,

Jonathan

 

Posted by: Jonathan Zhang
Post date: 1/11/2011 6:40:29 PM

RE: Solid Edge Addin Wizard for Visual C++ 2008

Valued Contributor
Valued Contributor

Misplaced during my last upgrade.  It has been added back.

 

 

Posted by: Jason Newell
Post date: 1/11/2011 7:14:54 PM